Select your region & language

AMR Sensors (Magnetic Sensors) FAQ QPermalloy

A

Permalloy is a nickel-iron alloy.

One characteristic of permalloy is that its resistance changes when subjected to a magnetic field from a certain direction. AMR sensors use this characteristic to function as magnetic switches. The resistance value changes by up to 3% based on the magnetic field strength and the direction of the magnetic force lines.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.