Select your region & language

CO2 sensor FAQ QDo we need to calibrate these sensors? How and when does the automatic calibration work?

A

These sensors calibrate automatically, so periodic manual calibration is not necessary.
The automatic calibration cycle is as follows.

  1. When initial stabilization has completed immediately after the power is turned on
  2. When 24 h ±10 s have passed since the previous calibration and when there has been a temperature change of 5°C or more since the last calibration

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.