Soil sensor FAQQWhat is the input voltage?

A

DC 3 V to 6 V. For the SLT5008 SDI-12 interface, the range is DC 9.6 V to 16 V.
Please check our product lineup information.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.