Select your region & language

Vibration Sensor Devices FAQ QWhat are the recommended land information and precautions for the vibration sensor devices?

A
  • Since TEST1 and TEST2 terminals are inspection terminals, short circuit between the two terminals on the board and do not connect them to other terminals.
  • Since the outer top and side surface except the bottom of the product are covered by shield electrode (the same potential as GND), design the substrate so that the opening land and the outer surface of the product are not adjacent as over resist.
Fig of Standard soldering pattern

Standard soldering pattern (Top View)
Opening Land Pitch : 1.85mm
Opening Land Diameter : 0.6mm

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.