NTC Thermistors FAQQ[NXF Series] What is the measurement temperature error at each temperature?

A

This varies with the characteristic. The temperature sensing accuracy of flagship product NXF*15XH103F series is within ±2°C in the temperature range of −40°C to +125°C. For another characteristic, contact us.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.