NTC Thermistors FAQQ[NC* Series] What are the temperature error factors in SimSurfing?

A

Includes 25°C resistance, B constant deviation and approximate calculation error. It is also possible to include variations in the fixed resistance and input voltage on the circuit by setting parameters.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.