PTC Thermistors (POSISTOR®) FAQQ[PTFL/PTGL Series] Are there any precautions to take when soldering to the leads of this PTC Thermistor?

A
This PTC Thermistor element and leads are soldered together. Because of this, solder the leads at a point 5mm or more away from the lead's root so that the joints between the element and lead are not affected. In addition, make sure that the soldering iron does not come into contact with the thermistor body.

Please be careful about the following points on implementing our product.

1.This product is using the solder of 221+/-5 ℃ of melting points, in order to connect ceramics with 
a lead wire. Do not heat up a terminal area of this product over 180 ℃.

2. Do not touch the resin case by soldering iron. The soldering point shall be min. 5 mm away from the
 root of lead wire. Please solder the following conditions.
        ・Iron Tip Temperature : 360 degree C max.
        ・Soldering Time       : 4 seconds max. / 1 terminal
        ・Number of Soldering  : 1

3.If you coat this product by resin, please evaluate the qualityl of this product before you use it.
The stress of fource which is caused by coating materials or heat cycles may cause failure 
mode such as deterioration of characteristic or current leak in worst case.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.