PTC Thermistors (POSISTOR®) FAQQ[PTGL Series] Though the operating temperature range is specified between -10°C and +60°C, can this range be widened?

A
When the operating temperature range is widened, the trip and hold currents are changed. Therefore, although great care must be taken, the range can be widened. For specifications, contact us.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.