| Consumer equipment |
CE |
Products that can be used in consumer equipment such as home appliances, audio/visual equipment, communication equipment, information equipment, office equipment, and household robotics, and whose functions are not directly related to the protection of human life and property. |
| Industrial equipment |
IE |
Products that can be used in industrial equipment such as base stations, manufacturing equipment, industrial robotics equipment, and measurement equipment, and whose functions do not directly relate to the protection of human life and property. |
| Automotive infotainment/comfort equipment |
AIC |
Products that can be used for automotive equipment such as car navigation systems and car audio systems that do not directly relate to human life and whose structure, equipment, and performance are not specifically required by law to meet technical standards for safety assurance or environmental protection. |
| Automotive powertrain/safety equipment |
APS |
Products that can be used for automotive equipment related to running, turning, stopping, safety devices, etc., or equipment whose structure, equipment, and performance are legally required to meet technical standards for safety assurance or environmental protection. |
| Medical equipment [GHTF A/B]
About the Classification of Applications of Electronic Components for Medical Equipment
|
MAB |
Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B, the functions of which are not directly involved in protection of human life or property. |
| Medical equipment [GHTF C]
About the Classification of Applications of Electronic Components for Medical Equipment
|
MC |
Products suitable for use in medical devices designated under the GHTF international classifications as Class C, the malfunctioning of which is considered to pose a comparatively high risk to the human body. |
| Medical equipment [GHTF D]
About the Classification of Applications of Electronic Components for Medical Equipment
|
MD |
Products suitable for use in medical devices designated under the GHTF international classifications as Class D, equipment that is highly invasive to the patient and the malfunctioning of which is considered to pose a direct danger to human life. |
| Medical equipment [GHTF A/B/C] except for implant equipment |
MeI |
- Applicable products
- Ceramic capacitors, Polymer Aluminum Electrolytic Capacitors
Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B (the functions of which are not directly involved in protection of human life or property) or in medical devices other than implants designated under the GHTF international classifications as Class C (the malfunctioning of which is considered to pose a comparatively high risk to the human body).
|
| Implanted medical equipment or medical equipment [GHTF D] |
MI |
- Applicable products
- Ceramic capacitors
Products suitable for use in implanted medical devices designated under the GHTF international classifications as Class C or Class D (the malfunctioning of which is considered to pose a comparatively high risk to the human body, or equipment that is highly invasive to the patient and the malfunctioning of which is considered to pose a direct danger to human life) or in medical devices designated under the GHTF international classifications as Class D (equipment that is highly invasive to the patient and the malfunctioning of which is considered to pose a direct danger to human life).
|
| Medical equipment [GHTF A/B/C] except for implant & surgery & auto injector |
MeS |
- Applicable products
- Inductors, Noise Suppression Products/EMI Suppression Filters, Baluns, Couplers
Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B (the functions of which are not directly involved in protection of human life or property) or in medical devices other than implant, surgery, and auto injector under the GHTF international classifications as Class C (the malfunctioning of which is considered to pose a comparatively high risk to the human body).
|
| Mobile Electronics |
ME |
- Applicable products
- Ceramic capacitors
When the specific application is only for mobile devices
Thermistors, Timing Devices, Polymer Aluminum Electrolytic Capacitors, Single Layer Microchip Capacitors, Silicon Capacitors, Variable Capacitors, TVS Diode, LC Baluns, LC Couplers, LC Filters, LC Diplexers
These products can be used in mobile equipment such as mobile phones, smartphones, tablet PCs, TV games / video games, cameras, electronic dictionaries, wristwatches, small servers, and IPC-9592B class 1 equipment, and in products whose functions do not directly affect the protection of human life and property.
|
| Consumer equipment - Differential Transmission |
CDT |
- Applicable products
- Common mode choke coils, Silicon Capacitors, TVS Diode
These products can be used in consumer products such as home appliances, AV equipment, communications equipment, information equipment, office equipment, and household robot equipment, and in the differential transmission circuits of products whose functions do not directly affect the protection of human life and property.
|
| Industrial equipment except for transportation & facility & energy equipment |
IeT |
- Applicable products
- Inductors, Noise Suppression Products/EMI Suppression Filters, Timing Devices, Baluns, Couplers
Products that can be used in industrial equipment such as base stations, manufacturing equipment, industrial robotics equipment, and measurement equipment, but except for transportation equipment, facility equipment and energy equipment, and also whose functions do not directly relate to the protection of human life and property.
|
| HDD |
HDD |
- Applicable products
- Shock sensors, Silicon Capacitors
These products can be used in impact detection in PC hard disk drives.
|
| Double feed detection |
DFD |
- Applicable products
- Ultrasonic sensors MA300D1-1, Silicon Capacitors
These products can be used in double-feed detection of paper sheets in printers, MFPs, and scanners.
|
| Automotive [Ask Murata] |
AaM |
Products for use in automotive.
For details on specific applications, please contact us.
|