Select your region & language

Vibration Sensor Devices FAQ QWhat is the dynamic range of the vibration sensor devices (full frequency range comparison) ?

A

Murata vibration sensor has Larger dynamic range than MEMS type at all frequency range.

Comparison of Murata’s vibration sensor & MEMS sensor

Murata
Resonant frequency characteristics Typ.+4dB (1.6 times)
Dynamic range at resonant frequency ±56.8[G] ÷ 1.6 = ±35.5[G]
MEMS sensor (ADXL1002)
Resonant frequency characteristics Typ.+12dB (4.0 times)
Dynamic range at resonant frequency ±62.5[G] ÷ 4 = ±15.6[G]

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.