Select your region & language

Vibration Sensor Devices FAQ QWhat is the recommended reflow profile for the vibration sensor devices?

A
Temperature profile of standard reflow soldering
Temperature profile of standard reflow soldering Pre-heat conditions 150 ⇛ 200°C 60 to 150s
Heating conditions More than 220°C 20 to 60s
Peak temperature 245±10°C

Precautions

  1. This product is designed on the premise of reflow solder mounting, and should not be joined by hand soldering or with conductive adhesives.
  2. Be sure to mount this product on a printed circuit board using a standard land pattern. If used by any other implementation method, performance is not guaranteed.
  3. If this product becomes high temperature beyond the limit even once, it loses piezoelectric properties and becomes non-functional.
  4. This product is easily affected by humidity, so we cannot recommend any washing. Please note that if you clean it, you will use it within the scope of your company's responsibility.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.