Select your region & language

Inclinometers FAQQHow does the frequency response look for Murata Electronics Oy's inclinometers?

A
In the SCA61T series the -3dB point is at 18 ±10Hz, 20dB/dec roll off. Attenuation at 1Hz is approx. 0,1% In the CBxH1G parts in the SCA610 series the -3dB point is at 6 ±4Hz, 20dB/dec, giving an attenuation of approx. 5,6% at 1Hz.