Select your region & language

Ceramic Resonators (CERALOCK) FAQQIs there any problem if CERALOCK is mounted in opposite direction?

A
In case of mounting CERALOCK in opposite direction, maximum 0.1% of frequency correlation may occur.
Customized part of tight tolerance series is made by adjustment of frequency on customer’s PCB. However, if you put it in opposite direction, it may be not able to meet required frequency tolerance. 
Please pay attention to the mounting direction when you mount CERALOCK on your PCB.

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
Does CERALOCK have orientation?
Q.
Why does frequency correlation occur when CERALOCK is mounted in opposite direction?
Q.
What are the meanings of the Marking?