Select your region & language

Inductors FAQQWhich RF inductor series is optimal for an impedance matching circuit?

A

An inductor used in an impedance matching circuit requires a low loss to transmit a signal efficiently.

Therefore, we recommend that you use an inductance value with a high Q characteristic. In addition, the matching accuracy decreases as it deviates from the required inductance.

Therefore, select a product with a narrow tolerance as needed.

Use the selection tool indicating the relationship between the size and Q value of the Murata RF inductor to select the product lineup that has the highest Q characteristics in the allowable size.