Select your region & language

Microblower FAQQCan multiple microblowers be driven in parallel in a single drive circuit?

A
No, it is not recommended.
The driving frequency of the individual microblowers is different. When multiple microblowers are connected to single drive circuit, it will cause the characteristics to deteriorate because the microblowers operate at a frequency different than the optimal drive frequency.