Select your region & language

AMR Sensors (Magnetic Sensors) FAQ QHow does the current consumption change based on the input voltage?

A
The input voltage and current consumption have a proportional relationship.
For example, the MRMS501A-001 identifies levels at 1.8V. At 1.8V, we have 3μA (typ), and so a current consumption operating at 3.5V, which is almost twice 1.8V, is about 6μA (typ).