Murata Manufacturing today announced the launch of the FTI Series (FTN21XH502F0SRU), a groundbreaking NTC thermistor that sets a new industry standard for automotive thermal management. The product is the world’s first to achieve both a resin-molded design and wire-bonding compatibility in a single thermistor. The integration of these two innovations provides unprecedented flexibility for designing and assembling printed circuit boards (PCBs), directly addressing the needs of modern automotive applications, including electric vehicle (EV) inverters and DC-DC converters.
Featuring a resin-molded structure, together with wire-bonding compatibility, allows for highly flexible installation directly on the PCB and in closer proximity to power semiconductor components. This advancement eliminates the need for dedicated sensor mounting pads, which have traditionally restricted layout options and increased board size. As a result, design engineers gain much greater freedom in PCB design, enabling more compact and efficient modules – especially important in modern EVs, where electronic controls must be highly integrated in tight spaces.
Another key strength of the FTI Series is its high-temperature operating capability. Leveraging Murata’s proprietary external electrode bonding technology, the thermistor ensures reliable performance in harsh environments, with guaranteed operation up to 175°C. This is among the highest in industry and is critical for next-generation automotive applications, especially within powertrains and other high-power modules where heat management is a constant challenge. With this level of heat resistance, automotive designers can ensure the safety, stability, and longevity of their systems even under demanding conditions, such as those found in EV inverters and DC-DC converters.
By enabling precise and rapid temperature measurement directly adjacent to semiconductor devices, the FTI Series allows for a reduction in temperature margins within a system’s design. This means that a power semiconductor’s performance can be maximized without over-engineering for excessive safety margins, creating opportunities to reduce the size of chips or the number of chips used in parallel, leading to smaller modules and lower overall costs. Further, this cost-saving feature does not come at the expense of reliability or performance, making the thermistor an ideal solution for manufacturers seeking to optimize their designs both technically and economically. The FTI Series is available in a compact 2012 mm / 0805-inch package and exhibits a resistance at 25 °C (R25) of 5 kΩ ± 1% with a B-constant (25 °C / 50 °C) of 3380 K ± 1%.
“In response to the increasingly sophisticated requirements of the automotive market, Murata remains committed to expanding its product lineup to include a broader range of resistance values and to offer new variations, such as silver sintering-compatible models in addition to traditional solder-mounted types,” said Munenori Hikita, Director of Functional Devices Division at Murata. He continued, “Through these ongoing efforts, and development of solutions like the new FTI series, Murata continues to support the advancement of EV technology and the broader automotive industry by delivering innovative, reliable, and cost-effective solutions.”
For inquiries or to request samples of the FTI series, please contact your local Murata representative or visit here.
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.