Select your region & language

Inductors FAQQWhat can happen when a product is used beyond the operating temperature range?

A
When a product is used beyond the operating temperature range, the following failures can be considered.
(1) Case where the coil is disconnected and results in an open mode
(2) Case where the insulation between the coils could not be maintained, and the inductance deteriorates
* Be careful not to use a product beyond the operating temperature range.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.