Select your region & language

Acceleration Sensors FAQQIf your resolution is 0.1% (of full scale) , it means that you have a resolution of 0.001*90 = 0.09 Degrees. However, your repeatability is 0.03 Degrees. How can repeatability be less than resolution?

A
It cannot be. The 0.1% resolution is the digital output resolution and the repeatability is measured from the analog output which has much higher resolution than 0.03 degrees. Based on the specification the analog output resolution over an 8Hz bandwidth is 20µg *sqrt (8) = about 60µg => 0.003 degrees. With this bandwidth the analog output resolution is 10 times better than the repeatability. From the digital output point of view the repeatability and the resolution are the same (±90 degrees = 180 degrees change. 180degrees/1,024=0.18 degrees/bit).

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.