Select your region & language

CO2 sensor FAQ QWhat are the operating temperature/humidity ranges? Can we use these sensors in environments with condensation or submerged in water?

A

The operating temperature range is −10 to +50°C. The operating humidity range is 0 to 95% RH (no condensation).
Condensation and submersion in water are prohibited. However, please consult with us if you intend to use these sensors in such an operating environment.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.