Select your region & language

Specific Applications Details

Swipe left or right to change screens View in landscape mode
Name Abbreviation Explanation
Consumer equipment CE Products that can be used in consumer equipment such as home appliances, audio/visual equipment, communication equipment, information equipment, office equipment, and household robotics, and whose functions are not directly related to the protection of human life and property.
Industrial equipment IE Products that can be used in industrial equipment such as base stations, manufacturing equipment, industrial robotics equipment, and measurement equipment, and whose functions do not directly relate to the protection of human life and property.
Automotive infotainment/comfort equipment AIC Products that can be used for automotive equipment such as car navigation systems and car audio systems that do not directly relate to human life and whose structure, equipment, and performance are not specifically required by law to meet technical standards for safety assurance or environmental protection.
Automotive powertrain/safety equipment APS Products that can be used for automotive equipment related to running, turning, stopping, safety devices, etc., or equipment whose structure, equipment, and performance are legally required to meet technical standards for safety assurance or environmental protection.
Medical equipment [GHTF A/B]

About the Classification of Applications of Electronic Components for Medical Equipment

MAB Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B, the functions of which are not directly involved in protection of human life or property.
Medical equipment [GHTF C]

About the Classification of Applications of Electronic Components for Medical Equipment

MC Products suitable for use in medical devices designated under the GHTF international classifications as Class C, the malfunctioning of which is considered to pose a comparatively high risk to the human body.
Medical equipment [GHTF D]

About the Classification of Applications of Electronic Components for Medical Equipment

MD Products suitable for use in medical devices designated under the GHTF international classifications as Class D, equipment that is highly invasive ​to the patient​ and the malfunctioning of which is considered to pose a direct danger to human life.
Medical equipment [GHTF A/B/C] except for implant equipment MeI
Applicable products
Ceramic capacitors, Polymer Aluminum Electrolytic Capacitors
Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B (the functions of which are not directly involved in protection of human life or property) or in medical devices other than implants designated under the GHTF international classifications as Class C (the malfunctioning of which is considered to pose a comparatively high risk to the human body).
Implanted medical equipment or medical equipment [GHTF D] MI
Applicable products
Ceramic capacitors
Products suitable for use in implanted medical devices designated under the GHTF international classifications as Class C or Class D (the malfunctioning of which is considered to pose a comparatively high risk to the human body, or equipment that is highly invasive to the patient and the malfunctioning of which​ is considered to pose a direct danger to human life) or in medical devices designated under the GHTF international classifications as Class D (equipment that is highly invasive ​to the patient and the malfunctioning of which is considered to pose a direct danger to human life).
Medical equipment [GHTF A/B/C] except for implant & surgery & auto injector MeS
Applicable products
Inductors, Noise Suppression Products/EMI Suppression Filters, Baluns, Couplers
Products suitable for use in medical devices designated under the GHTF international classifications as Class A or Class B (the functions of which are not directly involved in protection of human life or property) or in medical devices other than implant, surgery, and auto injector under the GHTF international classifications as Class C (the malfunctioning of which is considered to pose a comparatively high risk to the human body).
Mobile Electronics ME
Applicable products
Ceramic capacitors Read more When the specific application is only for mobile devices
Thermistors, Timing Devices, Polymer Aluminum Electrolytic Capacitors, Single Layer Microchip Capacitors, Silicon Capacitors, Variable Capacitors, TVS Diode, LC Baluns, LC Couplers, LC Filters, LC Diplexers
These products can be used in mobile equipment such as mobile phones, smartphones, tablet PCs, TV games / video games, cameras, electronic dictionaries, wristwatches, small servers, and IPC-9592B class 1 equipment, and in products whose functions do not directly affect the protection of human life and property.
Consumer equipment - Differential Transmission CDT
Applicable products
Common mode choke coils, Silicon Capacitors, TVS Diode
These products can be used in consumer products such as home appliances, AV equipment, communications equipment, information equipment, office equipment, and household robot equipment, and in the differential transmission circuits of products whose functions do not directly affect the protection of human life and property.
Industrial equipment except for transportation & facility & energy equipment IeT
Applicable products
Inductors, Noise Suppression Products/EMI Suppression Filters, Timing Devices, Baluns, Couplers
Products that can be used in industrial equipment such as base stations, manufacturing equipment, industrial robotics equipment, and measurement equipment, but except for transportation equipment, facility equipment and energy equipment, and also whose functions do not directly relate to the protection of human life and property.
HDD HDD
Applicable products
Shock sensors, Silicon Capacitors
These products can be used in impact detection in PC hard disk drives.
Double feed detection DFD
Applicable products
Ultrasonic sensors MA300D1-1, Silicon Capacitors
These products can be used in double-feed detection of paper sheets in printers, MFPs, and scanners.
Automotive [Ask Murata] AaM Products for use in automotive.
For details on specific applications, please contact us.
  • *Please refer to Our Website and specifications, etc. for information about the performance, functions, quality, management, and safety required for the above applications, and use Products after confirming the performance and reliability of the actual Product.

Caution : When the specific application is only for mobile devices<MLCC>

Mobile
Mobile application specific MLCC

Mobile application specific MLCC (products with specific applications only for mobile devices)
These MLCC products are designed for use in devices with a typical lifetime of less than 5 years.
(Examples: Cellular phone, Smartphone, Tablet PC, Digital camera, Watch, Electronics dictionary, Small-scale server, IPC-9592B class1 equipment, etc. )

Mobile application specific MLCC products are designed so that the estimated useful life can be extended longer than 5 years under the following conditions:
「80% of the rated voltage or less, Maximum operating temperature -20 degree C or less」 (10 years or more for general-purpose MLCC products). The estimated useful life under actual operating conditions can be approximated from the following chart.

* The estimated useful life is the time when the cumulative failure rate of continuous use is 1%.
* The estimated useful life data is provided for reference only. Please use it as a rough estimate when designing and using devices. The data is not intended as a guarantee of the product lifetime.
* If you have any questions, please feel free to contact us.

Lifetime of MLCC can also be estimated from voltage acceleration and temperature acceleration factors.
Please refer to following URL about these lifetime estimation.

Estimated useful life for mobile application specific MLCC Estimated useful life for mobile application specific MLCC