PTFL/PTFM Series (Overheat protection)
Q. What is the resistance-temperature characteristic?
Q. What is the characteristic at temperatures other than the sensing temperature?
Q. What is the thermal resistance of "POSISTOR®" with the object to be measured?
Q. Are these Series available in taping packaging?
Q. Are there any precautions to take when packaging "POSISTOR®" with resin?
Q. Are there any precautions to take when soldering "POSISTOR®" leads?
PTGL Series (Over current protection)
Q. How to select "POSISTOR®" for Over Current Protection?
Q. Is the Series available in taping packaging?
Q. Are there any precautions to take when soldering "POSISTOR®" leads?
Q. Doesn't "POSISTOR®" malfunction due to rush current or surge noise caused when supplying power?
Q. When current has a special waveform (pulse, etc.), how much are the trip and hold currents?
PRF Series (Overheat protection)
Q. Can this Series be flow-soldered?
Q. Can this Series be reflow-soldered twice or more?
Q. What is the characteristic at temperatures other than the sensing temperature?
Q. Are there any precautions to take when potting "POSISTOR®" with resin?
PRG Series (Over current protection)
Q. Can this Series be flow-soldered?
Q. Can this Series be reflow-soldered twice or more?
Q. How to select "POSISTOR®" for Over Current Protection?
Q. Are there any precautions to take when potting "POSISTOR®" with resin?
NTS Series
Q. Can the length of the leads be changed?
Q. Can the length of resin-coated type products be changed?
Q. Is this Series available in taping packaging?
Q. What is the measurement temperature error at each temperature?
Q. Are there any precautions to take when packaging this NTC Thermistor with resin?
Q. Are there any precautions to take when soldering to the leads of this NTC Thermistor?
NCP Series
Q. What electrode construction does the NCP Series have?
Q. Can the NCP Series be flow-soldered?
Q. Can this Series be reflow-soldered twice or more?
Q. What is the thermal time constant of this NTC Thermistor?
Thermistors