Wireless LAN (Wi-Fi) functions are increasingly being incorporated into many different products, such as mobile devices and printers.
However, if there is noise in the same frequency band as the Wi-Fi communication band inside a product, this will cause deterioration in the Wi-Fi communication characteristics.
Furthermore, the effects of very faint noise cannot be ignored in the case of self-inflicted interference problems arising inside the devices, and definitive ways of suppressing the noise are demanded.