Select your region & language

Ultrasonic SensorsOpen-Structure Ultrasonic Sensors

NRND *Please refrain from using these products as components in new models.

Ultrasonic sensors feature a composite oscillating body combining the oscillator — which joins a metal plate and piezoelectric ceramics — with a resonator. This body is elastically fixed to the base and housed in a case.

The resonator is shaped like a funnel to efficiently radiate the ultrasonic waves generated by the oscillating body into the air and to effectively concentrate ultrasonic waves from the air on the center of the oscillator.

“Sound pressure” is the most important parameter of open-structure ultrasonic sensors. In distance measurement applications, the higher the sound pressure of the ultrasonic sensor, the longer the sensor’s range.

Open Type
Development tool

Texas Instruments provide driving IC of ultrasonic sensor.

Please refer it for your evaluation and designing circuit of ultrasonic sensor.

Ultrasonic sensor IC site of Texas Instruments is hereOpen in New Window