CEATEC 2026
Advances in AI, robotics, and IoT are changing what is required from sensing technologies, creating new opportunities to detect, interpret, and act on physical conditions, material states, and biological signals with greater accuracy and efficiency. Addressing these evolving requirements, under CEATEC 2026’s theme “‘Transformation”’, Murata will showcase its latest technologies alongside innovative solutions developed in collaboration with partners. Together, the exhibits will highlight new approaches to sensing, monitoring, and detection that can help support a more connected, sustainable, and prosperous society of the future.
Murata exhibition details*1
- *1Exhibit items are under development, and product specifications and appearance are subject to change without notice.
Ultrasound Transmission Metamaterial
Murata’s ultrasound transmission metamaterial enables ultrasonic detection through materials such as metal and resin, which are normally difficult for ultrasound to penetrate. Applied to these obstructing materials, the metamaterial increases ultrasound transmission, extending ultrasonic sensing to applications where internal conditions have traditionally been difficult to assess, including nondestructive testing, flow meters and biomedical applications.
Related Links
Wearable Device for Capturing Trace Biomarkers*2
A wearable technology patch that enables highly accurate sensing of trace substances in the body, such as glucose and alcohol. Designed for advanced wellness and health monitoring applications, its proprietary enzyme-based sensing technology captures target substances, enabling accurate detection of trace biomarkers that were previously difficult to measure.
- *2 The exhibit showcases the technology and is not a finished product intended for medical use.
RFID Sensor Tag
A battery-free, wireless tag capable of sensing temperature, humidity, and strain. The technology enables real-time monitoring of conditions that have traditionally been difficult to assess, including bolt loosening and changes in concrete condition, and is designed to improve inspection and maintenance efficiency.
Related Links
Neuromorphic Sensing System
nspired by the information-processing mechanisms of biological nervous systems and sensory organs, this technology enables large-area, high-density sensing with ultra-low power consumption and low latency. Supporting applications like electronic skin for humanoid robots and equipment temperature monitoring, the system provides real-time detection of temperature distributions across a large surface area.
Obstacle detection for mobile robots equipped with thermophones
This solution equips a mobile robot with a thermophone, a device that generates ultrasound using heat, to detect nearby obstacles. It measures distances from 1 cm to 2 m and can detect transparent objects such as glass, which can be difficult for optical sensors such as cameras to identify. It can also operate in high-glare environments, supporting obstacle detection for mobile robotics applications.
Other Items
Murata will also showcase technologies that contribute in various ways toward fostering a sustainable and prosperous future society.
Details
| Session | October 13 (Tuesday) to October 16 (Friday) |
|---|---|
| Location | Makuhari Messe |
| Murata booth number | 7H340 |
| How to enter |
Pre-registration is required to enter CEATEC 2026. |
| Official Website | CEATEC 2026 |