TVS Diodes (ESD Protection Devices) FAQQCan reflow soldering be applied for diodes?

A

Available on all products.
Refer to this data sheet.

Soldering condition

Carefully perform preheating so that the temperature difference (ΔT) between the solder and products surface should be in the following range. When products are immersed in solvent after mounting, pay special attention to maintain the temperature difference within 100 °C. Soldering must be carried out by the above mentioned conditions to prevent products from damage. Contact Murata before use if concerning other soldering conditions.

Table of Soldering method and Temperature

Reflow soldering standard conditions (Example)

Swipe left or right to change screens View in landscape mode

Use rosin type flux or weakly active flux with a chlorine content of 0.2 wt % or less.

Related Links

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.