TVS Diodes (ESD Protection Devices) FAQ QMounting Position of TVS Diodes (ESD Protection Devices)

A
The ESD suppression effect is higher with pattern (1) in which the TVS diode is placed at the connector (entry point).
Pattern (2) is also effective in suppressing ESD, but less so than with pattern (1).
image of pattern (1)
image of pattern (2)
We give an image of ESD suppression with patterns (1) and (2) below.
The value that can be suppressed by the TVS diode is fixed. It is possible to release ESD further with a CMCC or similar.
image of ESD suppression with patterns (1) and (2)

Related Links

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.