Select your region & language

Inclinometers FAQQWhat is zero point and zero point (offset, bias) error?

A
The sensor is at zero point, when it is mounted in the prescribed position (measuring direction) and no acceleration is acting on it. For horizontal inclinometers and accelerometers it is at 0g (with the defined face up) and for vertical accelerometers at 1g. Zero Point Error is the deviation of the output, when the device is in its zero position, compared with the optimum value.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.