Inclinometers FAQQIs it also possible to get inclinometers with linearity error of no more than 0.5mg in ±0.1g measurement range and what is linearity change as a function of temperature (if any) ?

A
Yes, please ask the measuring results of linearity from Murata. Results are from between ±30 degree. For example in ± 0.1g measuring range the linearity is better than 0.5mg.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.