Select your region & language

Infrared Sensors FAQQWould detection distance be changed by temperature of the environment?

A
Yes, it changes. The output of the sensitivity of a pyroelectric infrared sensor changes due to the temperature difference between the background temperature and the object (people). For this reason, as the temperature difference becomes lower the change in the output also becomes lower in principle, and the detection range becomes shorter as a result.
There is no output of sensitivity when the background temperature is equivalent to the body temperature in principle. Since the surface temperature of a human body is uneven, the detector will never completely stop detecting in practical use.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.