Select your region & language

Ceramic Resonators (CERALOCK) FAQQIs there a limit to input voltage and signal?

A
The following table shows the maximum rating of CERALOCK about input voltage and signal. Please use CERALOCK under the following conditions.

Maximum Rating
Item Specification
D.C. Voltage D.C.6V max.
A.C. Voltage 15Vp-p max.
Withstanding Voltage
D.C.100V max.
5s max.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.