Select your region & language

CEATEC 2026

Main image of CEATEC 2026

Advances in AI, robotics, and IoT are changing what is required from sensing technologies, creating new opportunities to detect, interpret, and act on physical conditions, material states, and biological signals with greater accuracy and efficiency. Addressing these evolving requirements, under CEATEC 2026’s theme “‘Transformation”’, Murata will showcase its latest technologies alongside innovative solutions developed in collaboration with partners. Together, the exhibits will highlight new approaches to sensing, monitoring, and detection that can help support a more connected, sustainable, and prosperous society of the future.

Murata exhibition details*1

  • *1Exhibit items are under development, and product specifications and appearance are subject to change without notice.

Hand Tracking for Physical AI

This hand-tracking technology accurately captures subtle hand and finger movements without relying on external cameras. ContactGlove3 Pro, a hand-tracking glove developed by Melt Interface Technologies, incorporates Murata’s compact, high-sensitivity three-axis LF antenna. The captured motion data can support Physical AI applications such as robot learning, remote operation, and the capture of expert skill data in manufacturing.

Related Links

Image of Hand Tracking for Physical AI

Ultrasound Transmission Metamaterial

Murata’s ultrasound transmission metamaterial enables ultrasonic detection through materials such as metal and resin, which are normally difficult for ultrasound to penetrate. Applied to these obstructing materials, the metamaterial increases ultrasound transmission, extending ultrasonic sensing to applications where internal conditions have traditionally been difficult to assess, including nondestructive testing, flow meters and biomedical applications.

Related Links

Image of Ultrasound Transmission Metamaterial

Wearable Device for Capturing Trace Biomarkers*2

A wearable technology patch that enables highly accurate sensing of trace substances in the body, such as glucose and alcohol. Designed for advanced wellness and health monitoring applications, its proprietary enzyme-based sensing technology captures target substances, enabling accurate detection of trace biomarkers that were previously difficult to measure.

  • *2 The exhibit showcases the technology and is not a finished product intended for medical use.
Image of Wearable Device for Capturing Trace Biomarkers

RFID Sensor Tag

A battery-free, wireless tag capable of sensing temperature, humidity, and strain. The technology enables real-time monitoring of conditions that have traditionally been difficult to assess, including bolt loosening and changes in concrete condition, and is designed to improve inspection and maintenance efficiency.

Related Links

Image of RFID Sensor Tag

Neuromorphic Sensing System

nspired by the information-processing mechanisms of biological nervous systems and sensory organs, this technology enables large-area, high-density sensing with ultra-low power consumption and low latency. Supporting applications like electronic skin for humanoid robots and equipment temperature monitoring, the system provides real-time detection of temperature distributions across a large surface area.

Image of Neuromorphic Sensing System

Obstacle detection for mobile robots equipped with thermophones

This solution equips a mobile robot with a thermophone, a device that generates ultrasound using heat, to detect nearby obstacles. It measures distances from 1 cm to 2 m and can detect transparent objects such as glass, which can be difficult for optical sensors such as cameras to identify. It can also operate in high-glare environments, supporting obstacle detection for mobile robotics applications.

Image of Obstacle detection for mobile robots equipped with thermophones

Products and Solutions for a More Sustainable Environment

Other Items

Murata will also showcase technologies that contribute in various ways toward fostering a sustainable and prosperous future society.

Details

CEATEC 2026
Session October 13 (Tuesday) to October 16 (Friday)
Location Makuhari Messe Open in New Window
Murata booth number 7H340
How to enter

Pre-registration is required to enter CEATEC 2026.
Please complete "Pre-Registration" before visiting Makuhari Messe.

Official Website CEATEC 2026 Open in New Window
Floor map
PageTOP