Select your region & language

Murata Unveils Innovative 600W Open Frame Power Supply

  • Power Products

21-11-2024

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Murata Manufacturing Co. Ltd has expanded its line of open-frame AC to DC power supplies with the new PQC600. With its highly efficient and power-dense design, the PQC600 caters to the needs of the latest medical and industrial applications, such as hospital beds, dentist chairs, medical equipment, and industrial process machinery.

Compactness, reliability, and efficiency are paramount for contemporary power supplies. With its compact size and high-power density, Murata’s industrial-grade PQC600 is an ideal choice to fulfill these demands, offering 600W of power within a package that is less than 1U in height. Its dependable performance in medical and industrial settings is guaranteed through certification to the IEC 60601-1 Edition 3 medical safety standard, which includes 2 Means of Patient Protection (MOPP) from primary to secondary, 1 MOPP from the chassis to ground and 1 MOPP from output to chassis. Additionally, the PQC600 complies with the IEC 60601-1-2 4th Edition for EMC standards, ensuring robust electromagnetic compatibility, and is suitable for use with medical devices that have Type B or Type BF applied parts.

The PQC600 utilizes Murata Power Solutions (MPS) bespoke transformer design with an optimized layout and package design. With a 600W forced-air cooling design, it achieves an impressive efficiency of 95% at full load. The power supply features an optimized interleaved Power Factor Correction (PFC) and back-end synchronous rectification, all within a compact, layered design that ensures superior thermal performance. Furthermore, the PQC600 includes a droop current sharing feature, enabling multiple units to be configured in parallel for greater power scalability.

“Murata remains at the forefront of power supply innovation, creating denser and more efficient designs,” Tony Sharp, Director Product Marketing at Murata Manufacturing Co Ltd. “The innovative new PQC600 will help to drive progress across both industrial and medical sectors, benefiting a new generation of equipment.”

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter