Select your region & language

Started provision of the EVK-v2 equipped with the Renesas GreenPAK™ as a new evaluation board for the piezoelectric film sensor Picoleaf™

  • Sensors

16-10-2024

Murata Manufacturing Co., Ltd. (hereinafter “Murata”) has developed the “EVK-v2” evaluation board (hereinafter “this evaluation board”) for Murata’s piezoelectric film sensor Picoleaf™. The Evaluation boards includes Renesas Electronics Corporation (hereinafter “Renesas”) programmable mixed-signal GreenPAK™ IC and intuitively controllable GUI*. The Picoleaf can simplify function inspections compared to conventional evaluation boards, contributing to efficient product development. Provision will begin in October 2024.
Murata’s piezoelectric film sensor Picoleaf is a thin sensor with a thickness of 0.2 mm or lower, capable of detecting pressing force with its high sensitivity as well as bio signals and motion. Evaluation boards up to this point had fixed output analog signal amplification factors, requiring source code modifications to adjust the on/off determination threshold. Therefore, customers were required to perform sensitivity adjustments themselves and function inspections were complex.
In response, Murata developed this evaluation board that can variably amplify sensor signals from Picoleaf and convert them into output digital signals recognizable by a microprocessor. By adopting the Renesas GreenPAK, this evaluation board can simultaneously connect up to 4 channels worth of sensors. Additionally, the integrated GUI function has enabled the display of output analog signals, dynamic switching of the amplification rate, and adjustment of the threshold for on/off determination output, among other features. This evaluation board simplifies the evaluation of Picoleaf, contributing greatly to efficient product development.

  • *GUI (Graphical User Interface): A user interface that enables users to visually provide commands to the computer through the use of their mouse or a touch panel.

GUI sample of the evaluation board

Specifications of Murata’s evaluation board

Evaluation board name EVK-v2 (Product number: KT-DKPS017)
Renesas IC product number GreenPAK SLG47004V (subject to change without notice)
GUI Dedicated GUI available
Number of channels available for simultaneous evaluation 4 channels
Interface TYPE-C
Noise filter Available

Product pages

Click here for details on this evaluation board.

Related sites

Click here for details on the piezoelectric film sensor Picoleaf.

Inquiries

For inquiries on this evaluation board, see here.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter