The various characteristics of multilayer ceramic capacitors can be displayed in graphs.
Impedance, ESR, reactance, Q, dielectric dissipation factor (tanδ), equivalent inductance, equivalent capacitance, transmission characteristics (S21), reflection characteristics (S11), DC bias characteristics, temperature characteristics, ripple heat generation characteristics, and AC voltage characteristics
In the graph, the characteristics can be compared easily, because the characteristics of multiple items can be overwritten.
* In the XY axis of the graph, the Linear/Log can be switched and the display range can be set.