Select your region & language

Murata launches ultra compact low cost stand-alone LoRa module

  • Connectivity Modules

2016-07-19

We are planning to discontinue production of this item. (*Updated on April 2, 2026)

Murata today announced the launch of a compact low cost low power wide area network (LPWAN) wireless module that supports the LoRaWAN long range wireless protocol. This stand-alone compact module measures just 12.5 x 11.6 x 1.76 mm, is constructed in a metal shielded package and comprises a Semtech SX1276 ultra long range spread spectrum wireless transceiver and an STMicro STM32L0 series ARM Cortex M0+ 32 bit microcontroller (MCU). An integrated TCXO that has robust low drift thermal characteristics provides an accurate clock source for the RF transceiver.
Communication with the module can be achieved via UART, SPI, or I2C peripheral interfaces. An ADC and up to 18 GPIOs provide plenty of flexibility for connecting sensors, switches and status LEDs, and the module is powered from a 2.2 to 3.6 VDC supply. The Murata CMWX1ZZABZ-078 module has pre-certified radio regulatory approvals for operating in the 868 and 915 MHz industrial, scientific and medical (ISM) spectrum in most geographical regions of the world. 
The normal output power is + 14 dBm but a PA boost function can be selected to increase RF output to + 20dBm for long range applications or those where the end-device is sited in a poor signal location indoors.
The MCU includes 192 kB flash and 20 kB RAM, and has enough memory to embed customer applications and host other modulation stacks. In addition, an optional STSAFE secure element can be incorporated into the MCU to enhance the network security capabilities.

"We're excited to welcome a leader in wireless modules such as Murata into the LoRa ecosystem," said Marc Pegulu, Vice President and General Manager of Semtech’s Wireless and Sensing Product Group. 

"Since Murata joined the LoRa Alliance™, our teams have worked together to design a cost-effective, small form factor LoRaWAN™ module capable of supporting a wide range of sensors. We are confident Murata's new wireless module should help increase the adoption of the LoRaWAN platform worldwide, helping to make it the standard for LPWANs supporting low power IoT applications."

Typical applications for this module include smart metering, wearables, tracking, M2M and internet of things (IoT) edge nodes. Accommodating a wide range of temperatures, the module can operate from – 40 to + 85 °C.

Mass production will commence in November 2016, datasheet and samples will also be available around this time.

무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.