Select your region & language

Chip Ferrite beads BLM21SN/BLM31SN series supporting 8.5A/12A lines

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

2016-02-01

Chip Ferrite beads BLM21SN/BLM31SN series supporting 8.5A/12A lines

Overview

When it comes to chip ferrite beads for use in power supplies, one major criteria for their selection their high rated current value.

As such, Murata Manufacturing Co., Ltd has added chip ferrite beads that boast 8.5A and 12A ratings in the 0805 and 1206 chip sizes.

  

Background

Chip ferrite beads are used for either signal lines or power lines.

Of these two, when it comes to using the beads for power lines, the rated current value of the beads is extremely significant as an indicator that determines whether they can indeed be used. The maximum rated current value supported by conventional chip ferrite beads in the 2.0x1.2mm and 3.2x1.6mm sizes has been 6A.

By optimizing both materials and internal structure, Murata has now added chip ferrite beads with ratings of 8.5A and 12A to its line-up, thus extending the range of the products’ applications.

  

Features

Despite the small chip sizes of 0805 and 1206, the new chip ferrite beads successfully achieve the high rated current levels of 8.5A and 12A.

  

Applications

For suppression of noise in power lines

  

Parts List

  Applications   Parts List
 For general applications
 BLM21SN300SN1 (0805 size)
 BLM31SN500SN1 (1206 size)
 For automobile powertrain safety applications  BLM21SN300SH1 (0805 size)
 BLM31SN500SH1 (1206 size) 
 For automotive infotainment applications  BLM21SN300SZ1 (0805 size)
 BLM31SN500SZ1 (1206 size) 

  

Production

Mass Production 


무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.