Select your region & language

Murata introduces high-frequency chip inductors with high Q characteristics

  • Inductors

2016-03-14

​​이 제품은 NRND품입니다.
새로운 모델에 부품 채택을 삼가주십시오. (※2022년 6월 24일 업데이트)

Murata introduces high-frequency chip inductors with high Q characteristics

Overview

Murata Manufacturing Co., Ltd. has begun mass production  of the new LQP03TQ_02 series of compact 0201 standard size (0.6 x 0.3 x 0.3 mm) high-frequency chip inductors, which have some of the highest Q characteristics in the industry.

  

Background

With the increasingly more sophisticated functions being incorporated into mobile phones, demand continues to grow for inductors that are compact in size and have high Q characteristics. In terms of the company’s inductors in the 0201 standard size, the RF inductors in the LQP03TN_02 series have higher Q characteristics than the components offered on the market. 

As such, they are already being widely used, particularly in mobile phones, however, demand also exists for even higher levels of performance. To meet customer expectations, Murata is making available the LQP03TQ_02 series of high-frequency chip inductors with Q characteristics superior to those of its existing LQP03TN_02 series.

The new series is expected at some point to support even tighter tolerances (±0.05 nH) than before.

  

Applications

High-frequency modules for mobile phones (PA, ANT, SAW, GPS, etc.)
Smartphones, mobile phones (WCDMA, GSM, LTE, etc.)
W-LAN, Bluetooth® and other wireless modules
All types of high-frequency circuits

  

Parts List

LQP03TQ_02 series

Click here for details of the series lineup.

 

Production

Mass Production 


무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.