Select your region & language

Library of Dynamic Chip Inductor Models

  • Inductors

2015-07-27

Library of Dynamic Chip Inductor Models

Overview

On June 23rd, Murata Manufacturing Co., Ltd. publicly launched on its website a library of dynamic chip inductor models.


Background

In recent years, the use of circuit simulation has become widespread in the design of electronic devices. Manufacturers of electronic components support this trend by providing simulation models of their products. Most of these product models are what are called “static” models. They cannot reproduce dynamic phenomena such as changes in component characteristics due to fluctuations in the current value flowing through the component. Specifically, there is a significant divergence between the simulated values and the actual values when designing circuits where inductance DC superposition characteristics are a factor. Because of this, dynamic models that are capable of reducing the divergence between simulated and actual values are strongly preferred. 


About the newly launched library

This library contains dynamic models that take into account the phenomenon wherein the inductance changes with the current flowing through a chip inductor. These models enable simulations that appropriately reflect the characteristics of circuits in which the current changes over time.

[Series product numbers included in the library]
  • LQM series, 83 product numbers

[Download URL of supported simulator]
(Both inductor and MLCC products are included in a single library.)


Glossary

Product model
This refers to a set of data reflecting the characteristics of the components necessary for circuit simulation. The characteristics of each product number differ, so Murata prepares a separate component model for each product number.

DC superimposition characteristics of inductors
When a large current flows through an inductor with a core made of a strongly magnetic material (such as ferrite), the permeability of the strongly magnetic material drops as it approaches magnetic saturation. Due to this phenomenon, inductors using cores made of strongly magnetic materials such as ferrite are subject to variations in inductance when the size of the current flow changes. This is referred to as the DC superimposition characteristics of the inductor.



무라타에 대해서

주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.