Select your region & language

Inclinometers FAQQIn the SCA61T Series, the digital output has an 11 bit resolution. In the SCA 103T the resolution is 12 bits? Is this correct?

A
The effective digital output resolution of the SCA103T is really 12 bits. This is due to its X-X sensor configuration and the use of the two channels in differential mode. This is how the effective resolution of 12 bits can be achieved.