Select your region & language

TVS Diodes (ESD Protection Devices) FAQQWhy are bidirectional TVS diodes selected?

A

Images for unidirectional and bidirectional TVS diodes are indicated below.
Unidirectional TVS diodes are used in the reverse bias state. Line voltages for protection are between the 0 to VFWM range.
Therefore, it is basically applied for DC power line protection.
Bidirectional TVS diodes are capable of supporting both positive and negative electrodes. Bidirectional TVS diodes are applied as protection lines if applied on both positive and negative such as data lines.
Bidirectional diodes can be applied on DC power lines.

Images for unidirectional and bidirectional TVS diodes
Unidirectional
current starts to flow the breakdown voltage on one side.
Bidirectional
current starts to flow at the same voltage.

Related Links

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.