Select your region & language

Ceramic Resonators (CERALOCK) FAQQWhat is "spurious oscillation"?

A
In principle, the CERALOCK can be classified into two series: kHz-band type and MHz-band type. The product categories are identified by the vibration mode. However, any type of CERALOCK provides oscillation frequencies (parasitic oscillation) different from the main oscillation frequency. The oscillation with parasitic frequency is called spurious oscillation. You can check the behavior of the parasitic oscillation by using an impedance analyzer such as HP4294 (manufactured by Agilent Technologies).

Generally, any type of resonator provides odd-multiple overtone frequencies. However, the CERALOCK will rarely develop spurious oscillation due to overtone frequency, except for the resonators that inherently use the 3rd-overtone frequency, such as the CSTCW/CSACW_X Series (*1).

You can check the spurious oscillation due to overtone frequency by measuring the oscillation frequency. If the oscillation frequency is nearly triple the target frequency, it is regarded as spurious oscillation due to 3rd-overtone frequency.
When the CSTCW/CSACW_X Series is used, spurious oscillation with a fundamental wave (1/3 frequency) or quintuple wave (5/3 frequency) can be observed, because 3rd-overtone oscillation frequency is equal to its target oscillation frequency.

*1) CSTCW/CSACW Series
This product has been discontinued. We kindly request that you refrain from adopting it for new use.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.