Select your region & language

Ceramic Resonators (CERALOCK) FAQQIs there a recommended re-flow condition about SMD type CERALOCK?

A
We recommend the following soldering condition.
Flow soldering is not acceptable.

Recommendable Flux and Solder
Flux
Please use rosin based flux, but do not use water soluble flux.
Solder
Please use solder (Sn-3.0Ag-0.5Cu) under the following condition. Standard thickness of soldering paste: 0.10 to 0.15mm.

Recommendable Soldering Profile
Soldering Profile
Pre-heating
150 to 180゚C  ,  60 to 120 sec.
Heating
220゚C min.  ,  30 to 60 sec.
Peak Temperature
upper:260゚C  ,  1 sec. max.
lower:245゚C  ,  5 sec. max.

*Please refer to the following page for the recommended flow condition of lead type CERALOCK.
Q.Is there a recommended flow condition about lead type CERALOCK?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.