Select your region & language

Pyroelectric Infrared SensorsBasics - What is the Fresnel lens used in pyroelectric infrared sensors? -

At Murata, we offer Fresnel lenses with our pyroelectric infrared sensors.

What is a Fresnel lens?

A Fresnel lens is a type of flat lens which concentrically lines up many lenses with a triangular or other cross-sectional shape along a line. It is designed so that the light refracted by each triangle passes through the same point (focal point), and has the same function as a typical lens.
In a typical lens, the thickness of the material increases as you go from the periphery to the center. However, a Fresnel lens is unique in that because there is no change in thickness between the periphery and the center, it is thinner than a typical lens. Moreover, multiple lenses can be formed on one curved surface through resin formation.

Figure 1 of What is a Fresnel lens?

As shown in the figure below, a Fresnel lens is designed so that the rays pass through the same point (focal point).

Figure 2 of What is a Fresnel lens?

Why does an infrared sensor require a lens?

A pyroelectric infrared sensor must be used together with a Fresnel lens or other light-collecting components.

A Fresnel lens plays two major roles.

  1. Focuses the infrared rays
  2. Forms the detection area

Because the total energy of the infrared rays emitted from a human body is extremely low and the energy density decreases in inverse proportion to the square of the distance, the energy which enters the sensor is exceptionally small.
Accordingly, optical amplification in the form of a Fresnel lens is required for reliable sensor operation in each set.
When an optical system is not used in front of the sensor, the image of the sensor's directivity becomes an obscure blur of the nearby location, as shown in the figure below, and the detection area is not formed.

Figure 1 of Why does an infrared sensor require a lens?

Therefore, a lens must be used to focus the infrared rays on the element and increase the incident energy to the sensor.
In addition, the detection area can be formed by determining the angle at which the lens focuses the light.
That detection area is determined according to the combination of the sensor electrodes and the number of Fresnel lens segments.

Figure 2 of Why does an infrared sensor require a lens?