Select your region & language

Polymer Aluminum Electrolytic CapacitorsServer usage examples

Server market trends and challenges

Image of sever
Market changes: Higher performance driven by advances in generative AI and DX. Performance: Low voltage, large current and high stability. Roles of the capacitors: Low ESR, large capacitance, low profile and long life at high temperatures.

Against the backdrop of the acceleration in digital transformation (DX), the rapid spread of generative AI, and the expansion in the cloud service market, servers for data centers are being required to deliver computing performance and power supply capabilities far greater than conventional IT infrastructure. In particular, high-density servers equipped with numerous GPUs and AI accelerators are becoming the mainstream for AI workloads, including large language models (LLMs) and image and speech recognition applications. As a result, power consumption per server is increasing. This has meant that accommodating steep power supply loads involving very large currents flowing instantaneously has become a critical issue.

Current server challenges

In the latest CPUs, GPUs, and AI accelerators, operating voltages have been decreasing as semiconductor process technologies continue to scale down. On the other hand, higher computational density has led to current consumption reaching the level of several hundreds of amperes.
Therefore, the following characteristics are essential in server power supplies.

  1. Power supply stability capable of withstanding instantaneous large-current fluctuations
  2. Suppression of voltage ripples and drops
  3. High reliability and long life capable of withstanding operation 24 hours a day, 365 days a year

Moreover, the interior of servers features high-density mounting. This raises concerns about the heat generated building up inside servers. Consequently, there is demand for low-profile capacitors that can be mounted beneath heat sinks.

Roles of capacitors

As mentioned earlier, there has been a trend recently for higher performance driven by advances in generative AI and DX in servers.
Accordingly, components must possess the functions of low ESR, high capacity, low profile, and long life at high temperatures.

Features of Murata's polymer capacitor ECAS series

Murata's polymer capacitors have low ESR, low impedance, and have a high capacity.
Additionally, they are superior for their ripple absorption, smoothing, and transient response performances since there is no DC bias characteristic for capacitance and the temperature characteristic is stable.
Therefore, it is optimal for smoothing purposes in the input/output stage of power circuits and as backup for load fluctuation around the CPU.
This contributes to reducing the number of parts as well as the size of the circuit board area.

Example of applied circuit

You can use the ECAS series in circuits like those shown below.

Circuit diagram
Recommended part number
Volt. Cap. Part Number
2.5V 330uF ECASD40E337M006KA0
470uF ECASD40E477M4R5KA0
ECASD40E477V4R5KA4
ECASD40E477M006KA0
ECASD40E477V006KA4
6.3V 100uF ECASD40J107M015K00
220uF ECASD40J227M010KA0
10V 100uF ECASD41A107M015KA0
About the case size
Code L W T
D4 7.3±0.3 4.3±0.2 1.9±0.1

ECASD◯************ : D◯ is the dimension code.
(Ex.) ECASD40E477M006 / Dimension code : D4

Advantages of using the ECAS series

1. Low ripple noise

The ECAS series with its low ESR characteristics has excellent ripple noise suppression performance.

[Results of a simulation]

2. Voltage fluctuation stability with respect to load fluctuations

The ECAS series with its large capacitance characteristics features excellent stability with respect to load-side fluctuations in large-current applications.

When a tantalum capacitor is used
When the ECAS series is used

Comparison with other capacitors

Advantages over tantalum capacitors

Low ESR

The ECAS series has lower ESR compared to tantalum capacitors, which enables the realization of lower ripple noise.

Graph of low ESR

Reliability

The ECAS has more stable reliability compared to tantalum capacitors, which contributes to stable set operation.

Graph of reliability * Test condition: High temperature load