Since the ECAS series are low-profile components, they are capable of contributing to providing slim and stylish designs for monitors that use USB-PD.
Because of this, as is evident from its name, slim bezel monitors (frameless monitor), which are thin easy-to-see monitors with a wide display area, can be developed.
These monitors can easily be set up in offices with small work spaces.
Additionally, since remote work has become more common, there has been an increase in the number of people that have considered installing monitors for their homes to achieve higher work efficiency. Therefore, there is a high demand for slim monitors that can be installed in any location even at home. Additionally, since there are also portable monitors in the market that enable people to work away from home, we can say that there is a rise in demand for thinner monitors.
The ECAS has more stable reliability compared to tantalum capacitors, which contributes to stable set operation.
ECAS series capacitors burn less readily than tantalum capacitors, resulting in extremely low risk of ignition if a short occurs due to accidental failure.