Enter a product part number, or a portion of a part number.
Power over Coax (PoC) is a transmission method that enables the simplification of wiring by superimposing the power supply onto signal cables. By making use of suitable inductors from Murata’s extensive lineup, such as the LQW-F series developed for PoC applications such as ADAS camera interfaces, it is possible to create wide-band Bias-T circuits that employ fewer components. We recommend PoC for applications such as automobiles, industrial equipment (FA), robots, and drones. The “Bias-T Inductor Selection tool” on the Murata website can help you select the best components for your Bias-T circuits.
Enter a part number into the text box and click the “Search” button to search.
・An asterisk (*) and question mark (?) can be used as wild cards. When an asterisk (*) is entered in a character string where a portion of a part number being searched is unknown, products can be searched as a condition specifying any character string. A question mark (?) can be used as a condition specifying any character string.
Clicking the product name in the chart will display the applicable part number list.
When using the PoC (Power Over Coaxial) method, it is necessary to design Bias-T circuits to prevent high frequency signals from flowing into power lines that have low load impedance. Our Bias-T Inductor Selection Tool suggests the optimal component combination using an algorithm based on knowledge gained through application research.
Here we examine various simulation models (S-parameters, SPICE models, circuit simulation models, and electromagnetic field and thermal analysis simulation models <CAE>), selection tools, samples, and FAQs.
We take a look at the effects the pad and ground design have on the characteristic impedance, as well as measures to mitigate crosstalk.
Starts by answering the basic question “What is Power over Coax (PoC)?” and proceeds to a description of noise suppression examples.
Explains how to select components for Bias-T circuits used in deployment of Power over Coaxial (PoC) technology.
Describes Murata’s in-vehicle inductor products.
[From Beginners to Advanced Practitioners] We’re updating the webinars we have one after another! We explain the keys to noise suppression based on actual examples.
Automotive - AD/ADAS front camera - Power over Coax
Murata Community is a forum in which you can post questions about Murata products.
Learn more about Murata’s technologies.