Select your region & language

PTC Thermistors (POSISTOR)Operating curve / Current-time characteristics

Basic Knowledge of PTC Thermistor (POSISTOR)

Operating curve

Temperature of tripping PTC thermistor can be estimated by the operating curve.

How to create the operating curve

  1. Typical Dissipation Constant

    The typical dissipation constant is confirmed by measuring the current and the element temperature under the applied abnormal voltage in the environment where the set is used.
    (This is necessary because chip PTC thermistors have different the dissipation depending on their mounting condition.)

  2. Resistance value calculation

    The temperature of PTC thermistor calculate the resistance value using the following formula.
    Rx=(Abnormal Voltage)2/(typical dissipation constant ×(PTC heating temperature − Ambient Temperature))

  3. Check the intersection with resistance-temperature characteristics

    This is temperature of PTC thermistor that is tripped by an abnormal voltage.

Figure 1 : R-T characteristics and Operating curves

Current-time characteristics

It represents the relationship between the current and the time until the internal heat generation and external heat dissipation reach an equilibrium state for the application of a voltage above the maximum current.

Figure 2 : Operating time when applying exceeding the trip current

The larger applied voltage (current), the greater the instantaneous power consumption and the shorter the time to thermal equilibrium.

Operating Time

It is defined as the time until the inrush current reaches 1/2 value.

Figure 3 : Operating Time characteristics
Figure 4 : Inrush Current and Operating Time