Classification of Specific Applications of Electronic Components for Medical Equipment

We classify the specific applications of electronic components for medical equipment according to the international classification stipulated by the Global Harmonization Task Force (GHTF)*, and have set reliability standards and established quality systems according to their application.
Our quality system for each GHTF classification applies to electronic components for medical equipment, and does not guarantee suitability, performance, quality, etc. to the finished medical equipment application.

  • *The current activities have been replaced by the International Medical Device Regulators Forum (IMDRF).

Depending on the application of electronic components for medical equipment, malfunctions may directly endanger lives. If you intend to use our electronic components for medical equipment, please be sure to contact our sales representative to confirm the reliability standards and quality system for each product. If you use our electronic components for specific applications other than those for which they are intended, we will not be liable for any unexpected accidents or other damage resulting from such use.

In each country, classification has been stipulated for each finished medical equipment application, as shown in the examples below. Please contact our sales representative for information on the relationship between the laws and regulations of each country and the GHTF class.

  • Medical equipment in Japan is classified into Class Ⅰ, Ⅱ, Ⅲ, and Ⅳ according to the Act on Pharmaceuticals and Medical Devices (Act on Securing Quality, Efficacy and Safety of Products Including Pharmaceuticals and Medical Devices) stipulated by the Ministry of Health, Labour and Welfare.
  • Medical equipment in Europe is classified into Class Ⅰ, Ⅱ (a), Ⅱ (b), and Ⅲ according to the Medical Devices Regulation (MDR) stipulated by the competent authorities in the EU.
  • Medical equipment in the U.S. is classified into Class Ⅰ, Ⅱ, and Ⅲ according to the Federal Food, Drug, and Cosmetic Act (FFDCA Act) stipulated by the U.S. Food and Drug Administration (FDA).

Swipe left or right to change screens. View in landscape mode.
GHTF class Application Example Definition Applicable classes and the specific applications of our products
A Surgical microscopes and surgical lighting equipments Equipment that, in the event of a malfunction, is considered to pose an extremely low risk to the human body. Please contact us for details, as applicable classes and the specific applications differs for each product.
B Sphygmomanometers, diagnostic imaging systems, and thermometers Equipment that, in the event of a malfunction, is considered to pose a comparatively low risk to the human body.
C Insulin infusion pumps and glucose meters Equipment that, in the event of a malfunction, is considered to pose a comparatively high risk to the human body.
D Cardiac pacemakers and implantable defibrillators Equipment that is highly invasive to the patient and may directly lead to life-threatening consequences in the event of a malfunction.

Caution : When the specific application is only for mobile devices<MLCC>

Mobile
Only for Mobile devices

Mobile application specific MLCC (products with specific applications only for mobile devices)
These MLCC products are designed for use in devices with a typical lifetime of less than 5 years.
(Examples: Cellular phone, Smartphone, Tablet PC, Digital camera, Watch, Electronics dictionary, Small-scale server, IPC-9592B class1 equipment, etc. )

Mobile application specific MLCC products are designed so that the estimated useful life can be extended longer than 5 years under the following conditions:
「80% of the rated voltage or less, Maximum operating temperature -20 degree C or less」 (10 years or more for general-purpose MLCC products). The estimated useful life under actual operating conditions can be approximated from the following chart.

* The estimated useful life is the time when the cumulative failure rate of continuous use is 1%.
* The estimated useful life data is provided for reference only. Please use it as a rough estimate when designing and using devices. The data is not intended as a guarantee of the product lifetime.
* If you have any questions, please feel free to contact us.

Lifetime of MLCC can also be estimated from voltage acceleration and temperature acceleration factors.
Please refer to following URL about these lifetime estimation.

Estimated useful life for mobile application specific MLCC Estimated useful life for mobile application specific MLCC