Select your region & language

Polymer Aluminum Electrolytic CapacitorsMain applications and examples of use

Main applications

By adding the ECAS series to its line of multilayer ceramic capacitor (MLCC) products, Murata has further broadened the range of options available to customers. As electronic devices gain ever-more-sophisticated functionality, stricter voltage control is needed for the power lines of the CPU, etc. Maintaining voltage line stability sometimes requires large capacitance. In the past we would have suggested using multiple MLCCs, but now in many cases we can propose combining ECAS series capacitors with MLCCs in order to reduce both the quantity and cost of components.

Figure 1. Simplified Circuit Diagram of Power Line for CPU or FPGA

The ECAS series delivers low ESR, low impedance, and stable capacitance, making it ideal for applications such as smoothing (eliminating ripple and high transient response) various types of power lines subject to large fluctuations in the current load.
Basically, ECAS series capacitors are almost always used in combination with MLCCs, and the ECAS series capacitors really show their value in applications involving suppression of voltage fluctuations (high-speed back-up). Polymer-type tantalum electrolytic capacitors and polymer-type aluminum electrolytic capacitors (can-type) are widely used to suppress voltage fluctuations, but ECAS series capacitors are even more ideally suited for such applications due to their low ESR and good balance between ESR and capacitance.

If you are designing the power line for a CPU, we recommend the ECAS series.

Main markets

The ECAS series capacitors are widely used in products such as consumer applications (notebook PCs, LCD televisions, game consoles,etc.), Enterprise ones, Industrial ones and Network ones.

Swipe left or right to change screens View in landscape mode
Market Application Circuit Application
Consumer Internal connections
Notebook/Ultrabook Overall Power Management
  • Noise Suppression
  • Ripple Absorption
  • Decoupling
Power supply line around CPU,IC,etc Internal connections
USB Bus Power line  
CPU/GPU_PC
Panel_TV/Display (LCD/OLE)
Game Console
Wireless charger
IoT(UWB)
Drone
Enterprise Internal connections
Server
Enterprise HDD/SSD
Enterprise Display(LED)
Security(Camera/home)
Multi Function Printer
Smart meter
POS/Handy terminal
Industrial Internal connections
Production Equipment/module
PLC
Industrial PC
Robotics
Power tool
Network Internal connections
Base Station(wireless)
G-PON(Optical)
PoE
Switch/Router
others
Medical
IVI、V2X

Figure 2. Main Markets of the ECAS Series

Comparison of Application Performance

1. Good ripple absorption performance

Comparing voltage smoothing performance at the switching power output side with other capacitor types.

  • *This data is reference data

Figure 3. Good ripple absorption performance (2.5V/330uF)

2. Good transient response performance

Comparing transient response characteristics during quick load change with other capacitors.

Figure 4. Good transient response performance (2.5V/330uF)